11/18/2015 5:13 PM | |
Posts: 91 Rating: (4) |
Are they sure Update 5 for SP1 also doesn't have issues? Mine seems to crash a lot, Update 4 almost never crashed.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/19/2015 9:12:30 AMNew subject after splitting Last edited by: Min_Moderator at: 11/19/2015 11:11:41 AMChange title |
|
11/18/2015 6:05 PM | |
Posts: 5225 Rating: (1185) |
There is a 101 things that may cause software to not be responsive. For TIA one reason could be.. My personal experience is that Update 5 is more stable than 4 - for the work I use TIA for. Unhappily that does not mean that I now never have a software crash with update 5. What I do know is that there was some (unrelated to Siemens) software that my computer updated a while back that increased my problems. After doing a proper uninstall and install, the problem was sorted. I am of the opinion that the Siemens software likes to be installed alone on a PC. A virtual machine installation may be good for that. I recommend that if you regularly have issues, open a support request and see if the Siemens support guys can help you sort it out. w |
This contribution was helpful to1 thankful Users |
Follow us on