11/23/2015 5:26 PM | |
Posts: 1 Rating: (0) |
Hello, If PTO is not an option for an S7-1500, then what is the path forward to mimic the same behavior? I have code from an S7-1200 (v11) that uses PTO and need to mimic the same code on an S7-1500 (1511 specifically). I am very new to the Siemens world and need a 'quick and painless' way to use existing code. We do not have PROFIDrives. I am told by the manufacturer of the motor that the only way to control the motors is by Step and Direction. Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/24/2015 4:34:10 PMNew subject after splitting |
|
8/22/2017 1:15 PM | |
Posts: 19 Rating: (0) |
Hello! Do you have some example? Thanks! Bert regards Aleš |
8/22/2017 8:58 PM | |
Joined: 2/3/2011 Last visit: 6/27/2024 Posts: 346 Rating: (10) |
I think compact CPU´s has PTO outputs. |
8/23/2017 1:41 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by Ojstersek is split to a separate thread with the subject Need 32 PWM outputs for my aplication. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on