11/30/2015 2:52 PM | |
Posts: 57 Rating: (1) |
hello,
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/2/2015 10:11:05 AMNew subject after splitting |
|
12/2/2015 11:33 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
and some new points:
|
Last edited by: hdhosseini at: 12/2/2015 1:36:09 PM |
|
12/2/2015 6:28 PM | |
Posts: 57 Rating: (1) |
According to the very helpful link I ended up with those two pages (hand written). Does it look ok? Tomorrow I will program it in an STL block and call it in a OB35 with 10ms calling time. The coefficients a,b,c,d,e,g are still to be fine tuned so that the response is always stable and the output is an acceptable filtered outcome of an analog input. I am currently running some SIMULINK simulations to end up in something acceptable, as far as the coefficients are concerned. Hope it works..! AttachmentPictures.rar (78 Downloads) |
Follow us on