12/8/2015 8:56 AM | |
Posts: 11 Rating: (0) |
Hi Everyone I have a problem installing and upgrading my TIA V12 to TIA V13. What I have done already is uninstalling and reinstall all of the TIA V12 but if I begin to install Sinamics startdrive V13 it gives me the same error over and over. This is the same for any installation disc of TIA V13. Error description-"Failed to open windows installer database: C:\windows\installer\5e4e7.msi" I have a Simatic Field PG iCORE 7 64bit operating system. Also see attached the print screen. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/8/2015 11:37:57 AMNew subject after splitting |
|
12/8/2015 9:11 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, also run the installation as Admin, with Right-Click on Setup-> Run as Administrator. regards, |
FCK WAR! |
|
12/8/2015 9:47 AM | |
Posts: 11 Rating: (0) |
I have done it now, but still the same any other suggestions? |
12/8/2015 9:48 AM | |
Posts: 11 Rating: (0) |
@ChritophD @mopS4 |
12/8/2015 10:59 AM | |
Posts: 11 Rating: (0) |
FYI mopS4 |
12/8/2015 11:00 AM | |
Posts: 11 Rating: (0) |
FYI mopS4 |
Follow us on