12/9/2015 1:03 PM | |
Posts: 2 Rating: (0) |
Can you help me please. I want to control the Sinamic G130 by profibus via CU320. Communication with CPU 417 is good. I can see on PLC by profibus the Input Word 1:Drive status, Input Word 2: Drive Speed, Input Word 3: Drive Current, But how can I setup the VSD parameters to see the status of Digital input Status: DI4, DI5, DI5 and DI6 in input Word 4 PLC side. Merci. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/9/2015 3:53:54 PMNew subject after splitting |
|
12/11/2015 12:04 PM | |
Posts: 2 Rating: (0) |
Thank you very much. Wich value can I put in P0922? |
Follow us on