Industry Online Support
Technical Forum
3/1/2011 6:17 PM | |
Posts: 10 Rating: (0) |
Hello Friend, I am trying to make a connection b/w PLC S7 200 CPU 224 and PC, using WINCC Flexible 2008 RT via cable PPI cable USB/PPI. In WINCC: I set a button to InvertBit Q0.0 when click Connectino Menu: Communication driver: Simatic S7 200, Online ON HMI devide: Baud rate: 9600, add: 1 Network: Profile: PPI In PG/PC: access point of application: S7ONLINE (STEP7) PC/PPI cable But when i run HMI program in Runtime mode: error 190011 occur: value could not be written to PLC Can you help me to fingure out what problem may i have, and any solution if it's possible. Thanks so much for your help $ 140003 Gerneral connetion Error while going onlineWinCC Flexible advanced 2007with S7-200. Attachmentscreen.zip (145 Downloads) |
Last edited by: Dinesh Ramanujam at: 3/2/2011 3:37 AM |
|
3/2/2011 8:41 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread Runtime mode: error 190011 occur: value could not be written to PLC. Best regards O_Moderator |
Follow us on