1/4/2016 1:30 PM | |
Posts: 153 Rating: (9) |
Hello Can i connect with profinet integrated port in simotionD, if yes which hardware must be choose in simatic manager Thank ------------------------------------------------------------------------------------------ |
Last edited by: KhanhLe at: 1/4/2016 1:31:01 PMLast edited by: CS Moderator at: 1/4/2016 1:46:58 PMNew subject after splitting |
|
1/4/2016 1:56 PM | |
Posts: 153 Rating: (9) |
hello christophd hw selection i said is a blue circle in picture it's a CBE 30 card i want to know if use profinet integrated what i must choose |
1/4/2016 2:23 PM | |
Posts: 153 Rating: (9) |
Hello i have a simotion d435 training kit 6ZB2 470-0AE00, i think it not have CBE 30PN the project i download in topic Simotion D425 to S71200 TCP/IP communication. when i open project it automatically install GSDxml, the project use CBE 30PN so i want ask if use profinet integrated , which device i must use to replace CBE 30pn thanks |
1/5/2016 8:31 AM | |
Posts: 153 Rating: (9) |
Hello christophd I check a simotion and it not have a profinet integrated and CBE30 it only have 2 ie port so i think i will connect with s7cpu via Profibus, i think it easier than ethernet i try configure it, use i-slave Please check for me it right or wrong thank you AttachmentNew folder.rar (257 Downloads) |
Follow us on