1/18/2016 7:55 AM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (341)
|
Hi, It is mentioned in the help of this Function block VlvL: ------------- Neutral position This block provides the standard function Neutral position for motors, valves and controllers. The neutral position (de-energized state) is set using the SafePos parameter.
--------------- Thanks, HarrY |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
1/18/2016 1:57 PM | |
Joined: 12/16/2015 Last visit: 4/18/2024 Posts: 7 Rating: (0) |
yes they are working as expected |
11/8/2017 9:09 AM | |
Joined: 6/19/2017 Last visit: 4/30/2024 Posts: 7995 Rating: (163) |
New question published by Ajay5 is split to a separate thread with the subject Valve block input and output online values are not updating. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on