2/15/2016 10:08 AM | |
Joined: 8/26/2013 Last visit: 6/27/2024 Posts: 35 Rating:
|
Dear Sir, I have gone through control panel of drive (not the Axis), it shows error about License of Control Unit (D425-2) as below: Error A13000 License Not Adequate (0). When
I see the remedy for the problem, it shows additional licenses are
required & these must be activated via P9920 & P9921. But When I see the Expert List of Control Unit in SCOUT in ONLINE mode, both of theses parameters are not available there. The License Error file t is attached for your kind reference please. AttachmentControl Unit License error 0.docx (263 Downloads) |
This contribution was helpful to
1 thankful Users |
2/16/2016 7:23 AM | |
Joined: 8/26/2013 Last visit: 6/27/2024 Posts: 35 Rating:
|
Let me try with p10 & tell you the feedback |
2/16/2016 8:57 AM | |
Joined: 8/26/2013 Last visit: 6/27/2024 Posts: 35 Rating:
|
Sir, I have gone through all possible solutions. But Still the Problem was not solved. When I use Control Panel of Axis, it shows message "The switch-on of infeed is active" . When I use Control Panel of Drive, it shows message "The switch-on of drive is active" . What to do next. I am attaching you all the screen shots of my project including expert list of every module & Error occured. I am very much confused about Commissioning of the project. Attachment16.02.16.zip (241 Downloads) |
Follow us on