2/17/2016 12:22 PM | |
Posts: 1529 Rating:
|
No idea what gate current you need, but I would be going through an isolator first before I blow up my PLC wen it gets hit by 380V. What are you specifically trying to accomplish? You would probably be better off with a microcontroller like an Arduino or a PICT if you want to do a phase controller or something. |
2/17/2016 3:30 PM | |
Posts: 20 Rating:
|
I think that the gate is isolated within the igbt?? I need to switch 200vdc to a large eddy current brake. I have tested the pwm output with oscilloscope and it works fine without anything connected but when I try to raise the frequency above 100hz the output stops, do you have any idea why that is?? |
2/18/2016 5:31 AM | |
Posts: 1529 Rating:
|
No, your IGBT turns on with the voltage between Gate and Emitter. So, unless you are tying your PLC M to your 200V M (totally NOT advisable), then you need an isolator. Search for some IGBT gate driver circuits. |
Last edited by: Jeff Casagrande at: 2/18/2016 5:33:41 AM |
|
Follow us on