3/6/2016 4:39 PM | |
Posts: 1 Rating: (0) |
Hi, I have the following problem: I have a project in Tia Portal for CPU1214c, but i need to upgrade some code and the CPU is far from me and i can not connect directly. Can i save the new project in the MMC and send it to the technical people for insert it in the PLC?. How i can do?. Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/7/2016 10:37:02 AMNew subject after splitting |
|
3/6/2016 6:19 PM | |
Posts: 5225 Rating: (1185)
|
Yes you can use the MMC card. https://support.industry.siemens.com/cs/mdm/109478121?c=77327367435&lc=en-WW
Helpful? LATE NOTE: Also have a look at this write up.. |
Last edited by: William_B at: 3/6/2016 6:23:57 PM |
|
Follow us on