3/16/2016 5:12 PM | |
Posts: 1 Rating: (0) |
I have s7 315 2dp cpu which is password protected and i forget the password. I have backup of the program. Please tell me how can i remove the password. Best regards Gul Naseer ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/17/2016 1:11:20 PMNew subject after splitting |
|
3/16/2016 6:15 PM | |
Joined: 3/28/2015 Last visit: 5/4/2024 Posts: 721 Rating: (213) |
Hello, 1-Remove MMC out from CPU 2-Reset CPU 3-Insert MMC in the Simatic PG or in the Simatic USB prommer on your PC . 4-Open the Simatic Manager: Select" File"------ "S7 Memory Card" ------ "Delete" 5-Insert MMC into CPU 6-Download the program. 7-Save to Memory card. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on