4/22/2016 8:59 AM | |
Posts: 62 Rating: (0) |
Hello, We have turning maschine 840dsl with 3 axis x z and sp. The spindle is DC motor with ADI4 nad they have 4 gears i have a problem with gear change betwen execution of program. When i wont to facing a piece from 300 fi to fi 0. I put the cconstant speed in m/min. So that mean when i start facing on fi 300 fi is speed in rpm about 100, when i finishing in fi 0 is speed about 1500rpm. I want that machine before operation change to 4 gear, because now is start with gear 1 and they stop operation when they rache 450rpm(max speed in gear 1). Can somebody give me advice how to resolve this problem. p.s. sorry for my english. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/22/2016 12:27:40 PMNew subject after splitting |
|
4/22/2016 9:22 AM | |
Posts: 62 Rating: (0) |
I think that there can be a problem, that maschine must before operation check the maximum speed and they must change gear before operation? |
4/22/2016 10:00 AM | |
Posts: 62 Rating: (0) |
the spindle have 4 gears, if i try in mda m44 s1500 m3 the gear is change in 4 and the spindle speed is rached 1500rpm. |
4/22/2016 10:04 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Ok. Now in MDI just try following & check. S1500 M3 |
4/22/2016 10:06 AM | |
Posts: 62 Rating: (0) |
if now i try only m3 s1500 is working. so that mean that i must before operations call m40 to m44? |
Follow us on