Industry Online Support
Technical Forum
4/25/2016 6:54 AM | |
Posts: 7 Rating: (0) |
I am using S7 200 CPU Model 224XP with 2 port . I have to connect energy meter to one port and modem to another port what are the method to connect and what are the programming blocks to be used and how to program it so that energy meter data is can be read on Wincc through PLC and through modem program can be connected to winnc remortly . ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/25/2016 2:33:29 PMNew subject after splitting |
|
4/25/2016 4:38 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Posted twice, we are answered there: How to connect Energy Meter and Modem |
With best regards... |
|
Follow us on