(0)| 4/29/2016 11:29 AM | |
|
Joined: 3/19/2012 Last visit: 9/19/2025 Posts: 58 Rating:
|
It's not working for me as well. I'm using TIA Portal V13SP1. I've created an FC (not a DB) and I wanto to use a TON Timer, using a tag, declared in a GLOBAL DB, in SCL, and it doesn't work. I don't know why the same instruction in an FC ladder works, but not in SCL.... ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/29/2016 11:34:09 AMNew subject after splitting |
|
| 4/29/2016 12:02 PM | |
|
Posts: 84 Rating:
|
Hi, Try to declare your instance tag as InOut tag in your FC. Regards |
| 4/29/2016 5:12 PM | |
|
Joined: 3/19/2012 Last visit: 9/19/2025 Posts: 58 Rating:
|
How? I tried to declare an Input Output tag as IEC_TIMER, but this type of tag is not supported... |
| 4/29/2016 5:25 PM | |
|
Posts: 1250 Rating:
|
What doesn't work, can you be more specific and please post a snapshot of your TON declaration. Are all TON parameters assigned to tags?
|
| 4/29/2016 5:55 PM | |
|
Posts: 5225 Rating:
|
Hi. I have not yet had a reason to do this.. so I tried it. The instruction normally look like.. From a non-timer DB it would be like.. The other option via the INOUT is with the variable defined as TON_TIME type, and not IEC_TIMER. It can be defined as an INOUT and will compile for the declaration. Next I tried changing myTimer from IEC_TIMER to TON_TIME The last try was with the instructions.. w |
Follow us on