5/4/2016 12:14 AM | |
Joined: 9/27/2006 Last visit: 9/26/2024 Posts: 12283 Rating: (2685) |
Hello Arunraje; Based on the information in this link, the RTU560 is a substation monitoring unit: http://new.abb.com/substation-automation/products/remote-terminal-units/rtu560 These units generally use IEC 61850, IEC 870-5 or DNP3 for example in their communications. These are not protocols that WinCC SCADA supports directly, since it was designed for automation and process control. You will find a list of standard supported protocols in the attachment below. However, there are possibilities to incorporate substation protocols in WinCC, either through an add-on driver in some cases, or through WinCC versions produced by Siemens Energy, such as Sicam SCC (open the following link for more information): So please tell us what protocol you would like to use between your RTU560 and the SCADA system, and we may be able to provide more information. Hope this helps, Daniel Chartier |
Follow us on