5/14/2016 9:27 AM | |
Posts: 38 Rating: (2) |
Good day i would like to know if it is possible to control the Sinamic G110 with the SIemens S7-300 with both digital and analog inputs at the same time. The reason I want to know is because i want to control the speed of the Sinamic G110 through its analog input and through its digital inputs i want to control it's ON/OFF function and reverse function. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/17/2016 2:18:05 PMNew subject after splitting |
|
5/15/2016 12:02 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hello. Yes it is possible. Please see the connection examples in this manual |
Ayman Elotaify |
|
Follow us on