5/22/2016 1:44 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, Yes, you can use those infeed modules & drives. These are 611A analoge type, which works on DI/DO & with 10 V analog set point. Please download the below manual which will help you to understand the commissioning of this system. But for this you need servo motors with tacho or resolver feedback & not digital encoder. SIMODRIVE 611 analog, Transistor PWM Inverters for AC Feed Drives and AC Main Spindle Drives.HTH. |
This contribution was helpful to2 thankful Users |
Follow us on