6/17/2016 7:47 AM | |
Joined: 9/30/2013 Last visit: 8/23/2024 Posts: 7 Rating: (0) |
I am facing the same problem as sankannan. Using SFC 51 with SZL ID W#16#0692 or W#16#0292 does not help because it can only inform whether the ACT LED is on or off in that particular ET. Also, there are 2 ET in a rack for the two CPU in H-system. Both of them have the same diagnostic address. How will we get to know that the status is of ET in Rack 0 or ET in Rack 1? Please let me know If there is any way of getting the ACT LED status. ------------------------------------------------------------------------------------------ |
Last edited by: Akshita Saraswat at: 6/17/2016 7:47:41 AMLast edited by: Akshita Saraswat at: 6/17/2016 7:59:07 AMLast edited by: The Helping Hand at: 6/17/2016 10:38:36 AMNew subject after splitting |
|
Follow us on