7/10/2016 12:51 PM | |
Posts: 30 Rating: (2) |
Hi. I have a flowmeter with puls output, abt 930 pulses per liter. I have managed to arrange the total volyme, with counter and it´s quite simple, but i also want the momentary flow every minute. And there I have a slight problem because the momentary flow or rate needs to be "erased or updated" otherwise the momentary flow will not change so much when time have passed on to long. Im using a mathematic instruction and a timer, but sometimes when it resets, the mathematic instruction calculate it as a overflow because there´s no values yet. The counter is set to 1 with 10 pulses, easier during simulation. Does someone have a solution on this one? Attachmenttest flöde 2.zip (666 Downloads) |
7/10/2016 2:25 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078)
|
How many pulses are in a minute? |
7/10/2016 3:31 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078)
|
Here is a possible solution. She works to 30473 pulses per minute, or about 507 Hz. AttachmentFlow.zip (683 Downloads) |
This contribution was helpful to2 thankful Users |
7/10/2016 5:59 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078)
|
Hello William_B, you're have right. In the attachment the version with 10 seconds gate time. AttachmentFlow_V2.zip (635 Downloads) |
This contribution was helpful to1 thankful Users |
7/11/2016 4:12 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078)
|
4500 pulses per liter = 0.222 liters per pulse. Thus, a frequency of 175 Hz must be set in the simulation of I3 as a maximum. Please note: AttachmentFlow_V3.zip (823 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on