7/11/2016 5:12 AM | |
Joined: 2/20/2014 Last visit: 12/30/2024 Posts: 405 Rating: (38) |
Hi Pegaia, I had referred to the link that you had shared. But i am not able to do the backup as mentioned. Can you please advise? I am using a CPU1214 V2.2 (i have downloaded a program written using TIA V11). And i m trying to do the online backup using the TIA V13 SP1 update 7. Then appears a window saying that "Online backup is not supported".
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/11/2016 2:27:41 PMNew subject after splitting |
|
7/11/2016 6:57 AM | |
Joined: 5/12/2006 Last visit: 12/20/2024 Posts: 22482 Rating: (3040)
|
for a backup: 1.) Before this action you create an identical device configuration in the Project folder. Regards Christoph |
This contribution was helpful to1 thankful Users |
7/11/2016 7:42 AM | |
Joined: 2/20/2014 Last visit: 12/30/2024 Posts: 405 Rating: (38) |
Hi ChristophD, Yes i did that but i am getting that error message window while/after clicking on the upload button (in window which appears after i click on the "backup from the online device". Please advise. Thank you in advance.
|
7/11/2016 8:16 AM | |
Joined: 2/20/2014 Last visit: 12/30/2024 Posts: 405 Rating: (38) |
Hi ChristophD, Attached is the image of the error window. Thank you. |
Follow us on