7/11/2016 8:00 AM | |
Joined: 2/20/2014 Last visit: 10/8/2024 Posts: 396 Rating: (38) |
HI there, I would like to check something regarding the CPU with firmware version 4.1. I notice that i am able to download a program which has CPU 4.0 configured in the TIA V13 SP1 into a hardware with the firmware version of 4.1. Is this normal? This was done by mistake previously but i would like to know why there is no any message indicating the difference? What will be the effect if done this way? Any short/long term effect? What is the difference? Is there any effect? So far i notice there is no problem. Can anyone advice on these? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/11/2016 3:08:30 PMNew subject after splitting |
|
Follow us on