7/22/2016 8:26 AM | |
Posts: 9 Rating: (0) |
I have installed Adobe reader in F:\add_on I want to open this application from HMI using HSK10. For this i have changed the following: REGIE.INI in F:\Add_on [TaskConfiguration] Task10=name:=oemframe,cmdline:="F:\\add_on\\Reader\\AcroRd32.exe",PreLoad:=False,HeaderOnTop:=False,Classname:="AcroRd32",Timeout:=100000 OEMFRAME.INI in F:\user [AcroRd32] windowstyle_off=720896 nSwitchToTaskAfterTermination=-2 nInitshowMode=3 nshowMode=3 fforcetaskfocus=1 fsearchonlyForTaskwindow=1 LANGUAGE.INI in F:\mmc\language HSK10 = "Reader" after all these changes i started HMI . I got Reader as HSK10. I pressed that and message appeared Area Reader being loaded...In background Adobe reader page opened. But after some time i got the message Warning: Application didn't post initComplete. Press enter and continue. After enter i can use the application but i want to know the reason behind this as this error message took around 1 min to clear. By using Winlister i also checked the the class name as suggested i found the class name AcrobatSDIWindow. But by changing the class name i also get the same message. Moreover when Adobe reader opened its not coming in full screen. Vertical softkeys and lower menu options are coming over this. Kindly help me out. I also found changes in OEMFRAME.INI file after running this application as follows: [AcroRd32] windowstyle_off=720896 nSwitchToTaskAfterTermination=-2 nInitshowMode=3 nshowMode=3 fforcetaskfocus=1 fsearchonlyForTaskwindow=1 hOEMFrameWnd=40638 hOEMFrameTask=0D48 hOEMAppWnd=0000 hOEMAppTask=0 hOEMAppWndRelatedOEMAppTask=0000 hOEMAppThread=0001 Help plz Rajeev ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/22/2016 2:40:30 PMNew subject after splitting |
|
7/23/2016 4:39 AM | |
Posts: 9 Rating: (0) |
Anyone please help... |
Follow us on