8/2/2016 12:00 PM | |
Posts: 1 Rating: (0) |
From update TIA V13 SP1 upd9 the updater doesn't work. It writes error message: "Unable to connect to the server.". Has anyone the same problem? Untill the upd9 it has worked fine. For example with the update 8 it works well. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/2/2016 4:16:59 PMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
8/3/2016 8:51 AM | |
Joined: 7/9/2015 Last visit: 8/1/2024 Posts: 3902 Rating: (574) |
Hi, please check this FAQ: How do you start the ASU for the TIA Portal when the message appears indicating that no connection can be established to the server?Regards, Towome |
|
|
9/30/2016 8:04 AM | |
Joined: 2/18/2015 Last visit: 5/6/2024 Posts: 31 Rating: (6) |
I get that .NET security fault message to. On Windows 8.1 |
10/20/2016 9:59 AM | |
Joined: 1/12/2016 Last visit: 5/17/2024 Posts: 42 Rating: (4) |
Hi, I had the same problem. The solution in my company was to go under Windows domain. Try this, regards. |
4/5/2018 10:49 AM | |
Posts: 2 Rating: (0) |
try to disable windows firewall and try to update again. It worked for me... I use V13 SP1 Update 9 good luck. Ahmet. |
Follow us on