8/8/2016 3:57 PM | |
Posts: 1 Rating:
|
Hi everyone, I have the same mistake in the diagnostic part of my s7 300 plc , 315 cpu. I would post the event here , please notify me that if all of them are errors or not and if they are what are they ? Is there any handbook for these errors? I would appreciate if you could inform me about it. Diagnostic buffer of module CPU 315 Order No./ Description Component Version 6ES7 315-1AF03-0AB0 Hardware 1 - - - Firmware V 1.2.0 Rack: 0 Slot: 2 Event 1 of 10: Event ID 16# 4302 Mode transition from STARTUP to RUN Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Automatic warm restart after backed up power on Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Automatic warm restart after backed up power on Previous operating mode: STARTUP (warm restart) Requested operating mode: RUN Incoming event 10:25:30.911 PM 07/23/2016 (Coding: 16# 4302 FF68 C700 0000 0810 7710) Event 2 of 10: Event ID 16# 1382 Request for automatic warm restart STOP due to: Power failure Startup information: - Startup without modified system configuration - No difference between setpoint and actual configuration - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Automatic warm restart after backed up power on Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of the automatic startup type at power on: - Automatic warm restart after backed up power on Requested OB: Startup OB (OB100) Priority class: 27 Incoming event 10:25:30.888 PM 07/23/2016 (Coding: 16# 1382 1B64 C772 494E 0810 7710) Event 3 of 10: Event ID 16# 4301 Mode transition from STOP to STARTUP STOP due to: Power failure Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Automatic warm restart after backed up power on Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of the automatic startup type at power on: - Automatic warm restart after backed up power on Previous operating mode: STOP (internal) Requested operating mode: STARTUP (warm restart) Incoming event 10:25:30.807 PM 07/23/2016 (Coding: 16# 4301 FF46 C772 494E 0810 7710) Event 4 of 10: Event ID 16# 4358 All modules are ready for operation Operating mode: STOP (internal) Incoming event 10:25:30.020 PM 07/23/2016 (Coding: 16# 4358 FF44 C000 0000 0000 0000) Event 5 of 10: Event ID 16# 4357 Module monitoring time started Operating mode: STOP (internal) Incoming event 10:25:05.577 PM 07/23/2016 (Coding: 16# 4357 FF44 C000 0000 0000 0000) Event 6 of 10: Event ID 16# 4300 Power on backed up Previous operating mode: No voltage Requested operating mode: STOP (own initialization) Incoming event 10:25:02.617 PM 07/23/2016 (Coding: 16# 4300 FFF3 0000 0000 0000 0000) Event 7 of 10: Event ID 16# 494E Power failure Previous operating mode: RUN Requested operating mode: No voltage External error, Incoming event 10:07:15.059 PM 07/23/2016 (Coding: 16# 494E FF8F C000 0000 0000 0000) Event 8 of 10: Event ID 16# 4302 Mode transition from STARTUP to RUN Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Automatic warm restart after backed up power on Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Automatic warm restart after backed up power on Previous operating mode: STARTUP (warm restart) Requested operating mode: RUN Incoming event 09:59:14.403 PM 07/23/2016 (Coding: 16# 4302 FF68 C700 0000 0810 7710) Event 9 of 10: Event ID 16# 1382 Request for automatic warm restart STOP due to: Power failure Startup information: - Startup without modified system configuration - No difference between setpoint and actual configuration - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Automatic warm restart after backed up power on Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of the automatic startup type at power on: - Automatic warm restart after backed up power on Requested OB: Startup OB (OB100) Priority class: 27 Incoming event 09:59:14.378 PM 07/23/2016 (Coding: 16# 1382 1B64 C772 494E 0810 7710) Event 10 of 10: Event ID 16# 4301 Mode transition from STOP to STARTUP STOP due to: Power failure Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Automatic warm restart after backed up power on Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of the automatic startup type at power on: - Automatic warm restart after backed up power on Previous operating mode: STOP (internal) Requested operating mode: STARTUP (warm restart) Incoming event 09:59:14.293 PM 07/23/2016 (Coding: 16# 4301 FF46 C772 494E 0810 7710) ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/10/2016 9:14:13 AMNew subject after splitting |
|
7/24/2019 12:14 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, events in the diagnostic buffer are not only errors. The S7-300 events are described in this manual, chapter 35, events: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 hope this helps, regards, |
FCK WAR! |
|
Follow us on