8/13/2016 1:43 PM | |
Posts: 92 Rating: (5) |
Hi there I have a Acramatic 2100 vickers , the council was sleep for 4 year and Did not work but I have all backups. Well, first I connect Power supply to CPU cart and H.D.D then connect the monitor VGA (which is touch ). I set the inputs to J1(Input Pin 50) . [ PWR OK , green Led ] [ BB , red Led ] [ RT ,red Led ] [ vsFail , red Led ] , what is these ALM LED's Mean? I cant Find it on the internet . Thanks Regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/15/2016 9:33:28 AMNew subject after splitting |
|
9/10/2017 6:49 PM | |
Posts: 92 Rating: (5) |
Dear Pipmop33 Thank you Very much. It would be perfect, I'll Contact you as I start to work on my A2100 Controllers. Best regards Russell |
Follow us on