8/25/2016 9:14 AM | |
Joined: 5/20/2015 Last visit: 9/2/2024 Posts: 216 Rating: (3) |
hi guys, I Have a Laptop in which some WinCC license keys were installed, now that laptop has some malfunction so i can not boot window and can not transfer the license keys directly to other systems or USB stick. So i connect that laptop hard drive to other PC where ALM is already installed, now i have transfer 3 out of 4 license keys to USB pen drive which were in the D drive of malfunctioned laptop, but 1 that is WinCC Audit RC license key which is in the C drive of that Laptop is showing Status of NOT TRANSFERABLE. i tried by both cut-paste and simple transfer command method but it wont work, i want to know IS IT POSSIBLE TO TRANSFER NOT TRANSFERABLE KEYS BY OFFLINE TRANSFER METHOD. if it is possible then please guide how to to that, because i have tried by referring help documents but i really wonder about how to GENERATE REQUEST CODE, and how to load and what is ".aut" file stands for. please find screen shot. thank you.. ------------------------------------------------------------------------------------------ |
Last edited by: gabbar at: 8/25/2016 9:16:31 AMLast edited by: Min_Moderator at: 8/25/2016 2:50:12 PMNew subject after splitting Let's do it... |
|
9/21/2016 12:22 PM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello I Think the following article help you "How can you recover defective licenses and authorizations?". |
Follow us on