9/6/2016 2:07 PM | |
Posts: 215 Rating: (6) |
Hello, I'm having a similar problem. I configured an IPC to work as a server, and another one to be the client. It works perfectly after a rough start. But now I'm trying to use my engineering PC as a second client. I configured everything according to the instruction list on the support site, but my PC won't connect to the server. I can point to the mcx-file in the data system of the server, but when I try to 'open' it, I get the error message, that the project path is invalid. I don't really know what to do, since the first client has no problems in accessing the file and getting information from the server. Any ideas how this problem could be solved? Kind regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/7/2016 12:27:03 PMNew subject after splitting |
|
Follow us on