9/6/2016 6:04 PM | |
Joined: 7/14/2015 Last visit: 9/20/2024 Posts: 1 Rating: (0) |
Hi schufri, Where I can start service OpcUaServerWinCC? Thanks, AC ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/7/2016 1:18:34 PMNew subject after splitting |
|
11/17/2016 10:57 AM | |
Posts: 5 Rating: (0) |
The Service OPC UA ServerwinCC is Paused in the windows Services. Even I try to restart manually . It is not starting. what could be the problem. |
11/17/2016 1:00 PM | |
Posts: 5 Rating: (0) |
IF the Service is not Starting what is the Suggested Remedy to start the Service? Is it a problem with my wincc Professional Installation? |
11/17/2016 1:09 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
there is no problem!! Start the WinCC RT Professional with the activated OPC Channel and the service works. see also: |
This contribution was helpful to1 thankful Users |
11/18/2016 8:22 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735)
|
Hi ChristophD
you do not have to use the OPC Channel because its the OPC Client of WinCC Prof. As everyone said a lot of time before if you start the Runtime then the WinCC OPC Server runs! Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on