(0)| 9/7/2016 10:00 AM | |
|
Joined: 5/20/2015 Last visit: 1/14/2026 Posts: 221 Rating:
|
hello guys... Recently i have change the running SCADA PC system with WInCC v7.3 and Configured Simatic logon services, as per User Administrators Groups And user, it was running fine on previous PC but when i change PC with Identical HW and SW configuration And OS too, the User Authorizations property is not working After Restoring the back up on newer one PC whereas i have changed wincc sever name to PC name and Created users as per WinCC in the Windows users and configured them as previously in Simatic logon and added them to the Logon Administrator Group of Window. Now simply i am getting login in winCC Runtime with Simatic logon users which are identical to windows users, but i am not getting Authorization access to any picture or button or any object in the wincc Runtime, License are just transferred from previous to new PC and status is Okay. thank you.
Gabbar ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/7/2016 2:46:17 PMNew subject after splitting Last edited by: gabbar at: 9/9/2016 8:03:30 AMLet's do it... |
|
Follow us on