9/27/2016 4:27 PM | |
Posts: 2 Rating: (0) |
Hi, Finally how do you fixed the problem, I have a similar problem, I have a network proyect with 3x LOGO 8, 1x LOGO 7 and 1x HMI simatic ktp700, a LOGO 8 is in RUN mode and go STOP mode and I have to connect the PC to the network to get RUN mode again. This happends once per day. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/28/2016 9:32:38 AMNew subject after splitting |
|
9/27/2016 5:55 PM | |
Posts: 2 Rating: (0) |
0BA8.Standard V1.08.03 |
12/17/2019 11:50 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
The error occurs when the LOGO!s are networked, e.g. with another LOGO!, another PLC, an HMI or something else. |
12/17/2019 1:22 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Yes, you can do that. If the LOGO!s are not networked, ie work as "stand-alone", this error does not occur. |
Follow us on