10/1/2016 9:27 AM | |
Posts: 2 Rating: (0) |
hello, I have 2 CPU 315 DP, when I want to connect to the PC via MPI input controller I get the following error "The network contains SEVERAL Independent rungs". On the other controllers can access. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/4/2016 10:36:35 AMNew subject after splitting |
|
10/3/2016 8:37 AM | |
Posts: 2 Rating: (0) |
Hello, When connecting your computer and CPU me in on-line connection displays the following error.
AttachmentHelp_print screens.docx (229 Downloads) |
Follow us on