10/17/2016 8:54 PM | |
Posts: 1 Rating: (0) |
I use a G120 with a CU250S-2 for basic positioning with a motor and an encoder. I uses the active homing with a switch as reference point. The problem is homing. When axis reached the switch (reference point coordinate), the actual value (encoder position) is not set to this coordinate. Besides this, the homing starts as expected, speed and positioning. Have anyone an idea where to look. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/18/2016 2:04:42 PMNew subject after splitting |
|
Follow us on