10/31/2016 6:33 AM | |
Joined: 9/14/2016 Last visit: 1/22/2020 Posts: 59 Rating: (1) |
Hello. I use a Scalance X212 ethernet switch, here's a problem that the speed of FO port is slower than it's expected. The distance is about 200-250 m, according to the instruction the maximum transmission range (segment length) is 3 km. That's why I think the problem isn't with the cable's length. What should I do to increase the speed of this FO port? Or is there any thing which should be changed of port's properties in Web Based Management? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/4/2016 10:34:10 AMNew subject after splitting |
|
11/4/2016 12:53 PM | |
Joined: 8/21/2014 Last visit: 5/7/2024 Posts: 952 Rating: (13) |
Question was postetd three times. Please continue here: |
My Forum is the place to personalize your profile, |
|
Follow us on