11/14/2016 1:14 PM | |
Joined: 9/23/2005 Last visit: 9/20/2024 Posts: 4707 Rating: (721) |
Here. |
Regards, |
|
This contribution was helpful to1 thankful Users |
11/14/2016 1:15 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, nowhere at this time. Which information you need exactly, which code is displayed? Christoph |
6/21/2019 10:31 AM | |
Posts: 64 Rating: (2) |
Isn't there any documentation yet about the leds & 7 segment display on simotion? I have this situation in a D445-2 DP/PN. There no way to access to it (I used all Ethernet ports). I also used several CF backups I have and with all of them I get the same situation ... Thanks in advance AttachmentIMG_3659.MOV (321 Downloads) |
6/21/2019 10:44 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hi, all CF Cards without project? LED and 7 Segment are described in capt 9.1.1. Commissioning and Hardware Installation Manual Regards Christoph |
Follow us on