11/11/2016 10:49 PM | |
Posts: 1 Rating: (0) |
Hi, I need a GSD file for Simocode pro V, E10 revision ( 3UF7010-1AU00-0 ), I was looking for no internet, but I didn't find it. Help me please....... ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/14/2016 3:12:04 PMNew subject after splitting |
|
11/11/2016 11:40 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello; Open the same link that was proposed by Les Paul, and download the Simocode Pro V gsd file available there. http://support.automation.siemens.com/WW/view/en/113630 It should be compatible with your version,. This is part of the header information for that gsd file: GSD-File for Product SIMOCODE pro V with PROFIsafe Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/14/2016 4:43:30 PMIntegrated the original download link, after thread moved. |
|
This contribution was helpful to2 thankful Users |
2/15/2017 4:38 AM | |
Posts: 4 Rating: (0) |
Hello,
|
Follow us on