11/24/2016 10:55 AM | |
Posts: 2 Rating: (0) |
Dear KSN, I also have a problem during parameter changing of T400. I've already connected to T400 and changed some parameters in test mode (online status show). after that I disconnected the T400 and closed the program. The problem is I've deleted the project file by mistake. I tried to open the back up project file and changed parameter in offline mode then connected to the T400 again. there was a message unknown online changes. I want to know if I click on the update button what will happen? The parameters in T400 will be replaced? After updating done will T400 restart by itself? I don't want T400 to restart itself because T400 is using to control a machine it can't be shutdown. Thanks, Nukchan
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/25/2016 11:13:48 AMNew subject after splitting Last edited by: Min_Moderator at: 11/25/2016 11:14:34 AMTypo |
|
11/25/2016 6:13 AM | |
Joined: 8/25/2006 Last visit: 5/8/2024 Posts: 2203 Rating: (277)
|
Hello. Yes, it will be better to compile and download program. |
11/15/2017 2:27 PM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8026 Rating: (163) |
New question published by Ziemens is split to a separate thread with the subject Not able to upload parameters from T400 . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on