11/29/2016 1:08 PM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Hi, am also facing issue with batch system. (SORRY, I DON'T HAVE EXPERIENCE WITH BATCH, TRYING TO RESTORE THE SYSTEM..) installation- wincc 6.2 sp2, batch v7.0 sp1(not pcs7 batch, batch with wincc). system was working for 6-7 years and it got crashed last week. i have re-installed all the software and now wincc and batch is healthy. Earlier i have exported the recipe data(.sbx), batch backup (.sbb file) and kept as backup. After installing the new software, i imported the .sbx file. But while doing the recipe validation, it was giving batch instant error. Attaching few screenshots and log corresponding to the error..(config details.docx) Since it is giving trouble, i formatted and reinstalled again and tried to restore the .sbb backup. after that i could able to see all the recipes and can be released also. But while opening the recipe, getting error as attached..(Image file- batch error). there is only 2 windows user, both are users are member of all available groups. Any suggestions are welcome.. ------------------------------------------------------------------------------------------ AttachmentBATCH EROR.zip (54 Downloads) |
Last edited by: Min_Moderator at: 11/30/2016 1:53:02 PMNew subject after splitting
|
|
12/26/2019 7:09 PM | |
Joined: 4/28/2015 Last visit: 4/7/2024 Posts: 58 Rating: (2) |
I hope this helps you: Read page 15 (Backup and restore: Reusing SIMATIC BATCH data) of this Document: SIMATIC BATCH A5E00495287-01 You can download it from here: https://cache.industry.siemens.com/dl/files/330/24451330/att_106860/v1/bfmainb_e.pdf ------------- Don't forget the stars ;) |
Follow us on