(0)| 12/13/2016 8:02 AM | |
|
Posts: 6 Rating:
|
Hi i am also having some problems configuring this module. This is the firs time I work with modbus on Siemens... I have a CPU 315-2 PN/DP PLC and CP 341 RS422/485_1 with modbus master license instald on it, and 2 32 24 DI and 2 32 DO modules. I hava to use Modbus RTU RS 485 I cannot seem to communicate with my Modbus slave devices.... can someone help me with the configuration. Thank you ! ------------------------------------------------------------------------------------------ |
Last edited by: Rebbellyon at: 12/13/2016 8:05:40 AMLast edited by: Min_Moderator at: 12/14/2016 3:57:25 PMNew subject after splitting |
|
| 12/13/2016 9:12 AM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello, for first you need set proper cfg in CP341 module, depended to your needed protocol. In case of use as Modbus RTU Master select this option in protocol. Next you need set same communication cfg as is defined on Slave, or change in both devices to same if you need other values. You need use RK instructions, in this case look to TIA help with instructions, CP341 manual or Modbus RTU system manual, there you can see also deep description of parameters, status values. You can look to this topic, is depended to Step7 v5.x but can be useful for you: Modbus master on 6ES7-341-1CH02-0AE0 stops working |
Last edited by: Duris_I at: 12/13/2016 9:15:22 AMWith best regards... |
|
This contribution was helpful to
|
|
| 12/14/2016 12:30 PM | |
|
Posts: 6 Rating:
|
Hi Well actually the topic name was why i posted. As for the update i did all that, but no result.... Sorry if i upset you, that was not the intention. |
| 12/14/2016 2:53 PM | |
|
Posts: 6 Rating:
|
I can only share the document and an MB Pool Document as per equipment. It is relatively simple to access the information in it, I managed to communicate with another PLC (not SIEMENS). MB driver S7WFPA1X V2.6 code pieces... well there is nothing now. I tried to use Modbus_comm_Load and Modbus_master, I configured them as in the HELP but... no exchange... That is my problem that i do not know how to configure the CP module, and now to request R/W form the slaves..... AttachmentReceive Transmit Data.pdf (655 Downloads) |
Last edited by: Rebbellyon at: 12/14/2016 2:54:34 PM |
|
| 12/14/2016 3:24 PM | |
|
Posts: 3093 Rating:
|
Hello Rebbellyon, Regards, |
| 12/14/2016 3:36 PM | |
|
Posts: 6 Rating:
|
Hi, i tired it .... and it did not work |
Follow us on