12/15/2016 4:59 PM | |
Joined: 11/6/2014 Last visit: 5/7/2022 Posts: 19 Rating: (0) |
Hi all, I have a problem with the SF led, it still ON (red) although the system is working fine but I need to know why this happening. below is what I did: I made a network consist two cpus (315-2 pn/dp and 317-2 pn/dp), Phoenix inline ILB PN 24 DI16 DIO16-2TX, Scalance 208 and ET200M. Im reading signal from the Inline IO and using 317-2 to send it to 315-2 with the aid of BSEND/BRCV SFBs then to present the reading to the ET200M module. everthing is working fine. but the led still ON. I attached the diagnostic buffer (Message 6) is hoping someone can help me to find the cause. I know it something related to the IO module because the diagnose address belong to it. but I dont know who to solve it. Thank you in advance AttachmentDiagnose.txt (297 Downloads) |
12/13/2017 8:22 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Ocandies is split to a separate thread with the subject Reset CPU317-2DP and now getting a System Failure light. Best regards |
Follow us on