12/23/2016 2:31 PM | |
Posts: 69 Rating: (0) |
hello everybody, i have one message from my automate siemens s5-100u cpu 103 on the display op7 so the message is : "$ 613 DB-Fehler Nr. 10 ( 0;10)" Thanks in advance for you help! norimane ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/25/2016 9:33:35 AMNew subject after splitting |
|
12/23/2016 7:13 PM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following topic: Error $ 613 Cause:Data block not available or too short. Remedy:Create data block of required length on the PLC. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
1/24/2017 1:48 PM | |
Posts: 30 Rating: (2) |
Hi. Ok. Im on my way to learn the S5-system, and past weeks i have test Communication between an old OP5 and S5-95. If you have done something with an S7 and a modern hmi, then you it´s quite simple to get the Communication to work. but it´s a Little bit different on the S5 Is it a AS551 Connection? or is it profibus? If AS551 the S5 needs an Communication driver in form of an functionblock (FB51) made by Siemens. Dont remember the file name but it´s on the internet :) Take a look into this one, chapter 3 for AS511, side 10-7 shows program for cpu restart. but you need to add L KY 51,0 between JC PB 51 and ju FB 51 in OB1 https://support.industry.siemens.com/cs/attachments/1137086/Kom_e.pdf The pdf also mention profibus. etc. Hope this helped a Little bit, but i am also new to this. |
Last edited by: Min_Moderator at: 1/24/2017 4:55:40 PMReplace link |
|
1/25/2017 6:48 AM | |
Joined: 5/6/2010 Last visit: 6/21/2024 Posts: 1968 Rating: (274) |
Hello, here is your requiered link https://support.industry.siemens.com/cs/document/1137086/communication?dti=0&lc=fr-WW And here a small hint if you need manuals in different languages: - open the document in the "wrong" language and look at the first page left below I hope this helps regards, |
This contribution was helpful to1 thankful Users |
Follow us on