1/4/2017 12:35 AM | |
Posts: 1 Rating: (0) |
Hello Brothers Open PMC 104 After Bios configuration the unit is start and stopping frequently advice what I have to do please Best regards Faris ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/5/2017 9:24:53 AMNew subject after splitting |
|
1/4/2017 11:05 AM | |
Posts: 111 Rating: (15) |
Hello fabsheru, the post is 6 years old. Open PMC isn't support since 2014, see here as an example: https://support.industry.siemens.com/cs/ww/en/pv/6EQ2008-2AA07-3BA0/pi Also there is no more online information available about the system. Because your issue: Change your BIOS settings back to the further configuration with which the system worked correctly. For such an old system, the main tip is: Never change a running system. Also perhaps a migration of the system to the supported system PCS 7 might be an idea. Anyway, I hope the answer could help you a little bit. |
Follow us on