1/20/2017 7:34 AM | |||||||||||
Posts: 1 Rating: (0) |
Hi We are suppose to communicate with Y Link 6ES7197-1LA12-0XA0 which has below components.
Pls support with valid GSD file for above Y Link used for SIMOCODE PRO-V communication with 3rd party master (non SIEMENS) Profibus DP. Regards DM ------------------------------------------------------------------------------------------ |
||||||||||
Last edited by: Min_Moderator at: 1/20/2017 10:09:24 AMNew subject after splitting |
|||||||||||
5/31/2017 3:35 PM | |||||||||||
Joined: 10/18/2014 Last visit: 9/16/2024 Posts: 95 Rating: (15) |
Hi i saw this late sorry, but reply may help in future to someone, you don't need GSD of Y-Link part number "6ES7197-1LA12-0XA0" you have to use IM153-2 --> 6ES7153-2BA70-0XB0 in hardware of program for configuration of your standalone profibus stations like simocode pro-v DP or any other IO station with single profibus port and you wanted that station to connect to S7-400H system. you dont need to configure Y-coupler during hardware config in program (simatic manager V5.x) you will find all configuration options of Y-Link in IM153-2 above mentioned, and you have select this IM153-2 from "PROFIBUS DP-- DP/PA Link-- IM153-2 OD" please find attached image from hardware configuration from simatic manager for y-link. you have option there to configure IM153-2 Red bundle as well as Y- coupler profibus addresses and assign I/O station on Y-coupler profibus subnet as per your station ( Simocode / DP supported single IM) Note: but only you cant assign more than 200 I/O bytes for Y-Link station you can check its manual detailed configuration and assignment I hope you have already completed your task thanks Ganesh Dighe |
||||||||||
Ganesh-0220 |
|||||||||||
This contribution was helpful to2 thankful Users |
Follow us on