Industry Online Support
Technical Forum
2/9/2017 10:13 AM | |
Posts: 4 Rating: (1) |
Hello all ! Nice Greetings. I am facing some problems with SIMIT simulation and hope you can help me . Very first question is, If it is possible to Simulate data from devices Eg (Siprotec Relay) which are connected over Y-Link to H-Stations in SIMIT? I am using SIMIT V7.1.0.4195 with Step 7 V5.5 + SP3 and CPU 414-5 H PLC in a redundant configuration. Please Check the attached images for the configuration I am using. My problem is I am not able to get the address of devices connected over Y-Link into SIMIT. Example from Image: I want to write Input 2001 from SIMIT into PLC, this address is of a Profibus slave device connected Via a Y-Link. Although this address is available in symbol table I can’t access it in SIMIT. Also device connected Via Y-Link cannot be expanded/ seen in the gateway area in SIMIT. If it is possible can you please help guide me what are the things I could do? If there is any more information required for clarification please let me know.
AttachmentSIMIT Simulation Issue.zip (45 Downloads) |
This contribution was helpful to1 thankful Users |
2/9/2017 4:43 PM | |
Posts: 4 Rating: (1) |
Well Actually it works! Regenerated all the files and downloaded everything from scratch. And It worked. |
Follow us on