2/9/2017 4:30 PM | |
Joined: 3/5/2015 Last visit: 10/9/2018 Posts: 5 Rating: (0) |
Dear All, I'm currently experiencing an interesting issue with PLCSIM V13 and wondered if someone could help. The issue is as follows; Load PLCSIM V13 and set simulation running, all OK Download software and hardware config and all starts up OK When running the simulation and going online with TIA Portal V13, the following happens to a few random networks and they do not function correctly, please see attached image. This is the first issue I've had with PLCSIM V13 so I count my blessings, but this is annoying as I cannot fully test the software at the moment.......:( Hoping to hear from you guys soon. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/10/2017 1:04:46 PMNew subject after splitting |
|
2/15/2017 9:17 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (152) |
There is no description about the problem, just a screenshot. I don't see any problem. |
2/16/2017 5:22 PM | |
Joined: 3/5/2015 Last visit: 10/9/2018 Posts: 5 Rating: (0) |
Hi, Thanks for responding, I am currently using windows 7. Kind regards. |
Follow us on