2/27/2017 12:11 PM | |
Joined: 2/8/2011 Last visit: 9/7/2023 Posts: 87 Rating: (8) |
Dear All, I have a project with version 6.1. This project needs to be upgraded to version 8.2. That's why I need support. How can I upload the project and in what order? Can I upgrade directly to Version 7.1 den Version 8.2? What is the path to this step by step? Greetings. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/28/2017 12:00:25 PMNew subject after splitting |
|
2/27/2017 2:15 PM | |
Joined: 6/14/2006 Last visit: 6/17/2024 Posts: 301 Rating: (60) |
Hi, there are two very good manuals available for upgrading to PCS 7 V8.2. If you do not want to use the new functions: http://support.automation.siemens.com/WW/view/en/109485952 If you want to have all of the new features after the upgrade: http://support.automation.siemens.com/WW/view/en/109485962 Hope this helps. Myst |
2/27/2017 3:10 PM | |
Joined: 2/8/2011 Last visit: 9/7/2023 Posts: 87 Rating: (8) |
Thanks for your fast answer..
|
3/1/2017 1:59 PM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191)
|
If you need PCS 7 versions and licencies for PCS 7 versions between V6.1 and V8.2 to upgrade you PCS 7 version you can order the service "SIMATIC Software Platform as a Service". SIMATIC Software Platform as as Service offers a cloud-based IT infrastructure with pre-installed and pre-configured SIMATIC engineering software. Benefit from the centrally available software on demand, for modernization and updates of the SIMATIC applications, even over several software versions. Link to SIMATIC Software Platform as as Service |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
Follow us on