3/8/2017 10:30 PM | |
Posts: 3 Rating: (0) |
Dear all, I have big problem. I am using PCS7 v6 (1) i make some modification in my logic (2) after finishing i make compile and it successfully. (3) Whem making download i face problem that some FB cant copied to CPU and cant download (4) my CPU now in stop mode and giving internal fault Pls i need help ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/9/2017 1:05:57 PMNew subject after splitting |
|
3/9/2017 9:25 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, Can you be more specific? What changes did you make exactly? A wild quess: You created a FB with a number higher than 2048 in a CPU other then a CPU410 or 417. That is a problem. Let me know the exact changes you made |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on