3/11/2017 1:10 PM | |
Posts: 1 Rating: (2) |
Hi, I have a problem to open a project v13 via TIA v14. 1-when open the project v13 seen message for upgrade to v14 then confirm to do . 2- attachment : step 2 3- in progress - attachment : step 3 4- failed - attachment : step 4 please help ------------------------------------------------------------------------------------------ AttachmentSteps.zip (447 Downloads) |
Last edited by: Min_Moderator at: 3/13/2017 10:55:46 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
3/11/2017 5:02 PM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following topic: Note More information is available in the internet under: |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
9/21/2017 10:25 PM | |
Posts: 3 Rating: (1) |
Dear all, I'm also experiencing problems converting a project from V13 SP1... Attached is the log file printed as PDF (it does not accept the original XML...) Any hints? AttachmentlogConversion.pdf (487 Downloads) |
9/22/2017 3:00 PM | |
Posts: 3 Rating: (1) |
Hi Christoph, attached are the packages for both systems. There are some differences but those packages are not used in the project (Simocode, Startdrive). Thanks for your help. Regards, Tomás AttachmentPackages.zip (307 Downloads) |
9/28/2017 12:58 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8192 Rating: (169) |
New question published by dgbach is split to a separate thread with the subject Where to find the problem in the V13 project?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on