3/10/2017 10:49 AM | |
Joined: 2/16/2017 Last visit: 6/6/2023 Posts: 15 Rating: (2) |
Can you tell, is it possible to activate independent screen window from other screen? I have a button with code:
It works only when independent screen window ("Screen window_1") belongs to screen from which this code is called. But if I execute it from another screen, it does not work. Is it possible to use the same screen window in all of screens in the WinCC Prof project (TIA V14)? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/13/2017 4:59:28 PMNew subject after splitting |
|
Follow us on