3/10/2017 2:36 PM | |
Joined: 12/15/2011 Last visit: 9/23/2023 Posts: 6 Rating: (0) |
Hi, I want to do the same. I have a DB with UDT's In the HMI I want to create a multiplexed tag with an index to connect the PLC DB. I have installed TIA Portal V14 update 2. When I tried to program the example at the help file I get the message UDT types are not permitted. I hope there is a solution for this. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/13/2017 5:43:59 PMNew subject after splitting |
|
Follow us on